User Activity

Posted on March 28, 2013 at 16:48 Error for foc sdk v3.2 Hello, I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error : C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC...
Posted on March 28, 2013 at 16:47 Hello, I compile the library foc sdk v3.2 with Atollic for stm32f100b and with gnu I have always the same error : C:\VSS\MC\3PH\012\SOFTWARE\FIRMWARE\MC SDK v3.3\MC library\src\MotorPowerMeasu...
Posted on October 26, 2012 at 13:20Hello, I work with stevalifn003v1. When I'm looking the output signal from the micro (on JP1,2,3,4,5,6) to the driver l6230, 3 are constant and 3 are PWM. This signals goes to logical gate on driver. If I want to w...
Posted on October 01, 2012 at 13:36Hello, In datasheet um1052, chap 5.2.3, there is a method to determine the hall phase shift. I have a delay between the max of emf1 and the rising edge of hall1, but if I have a delay and an angle, I can know the s...
Posted on September 25, 2012 at 15:40Hello, I have instal the st motor control workbench for steval ifn003v1. I have install the driver : ''Silicon Lab CP210x chip''. When I generate H. files, i'm going to monitor, but I have always the same error :...