2012-10-26 4:20 AM
Hello,
I work with stevalifn003v1. When I'm looking the output signal from the micro (on JP1,2,3,4,5,6) to the driver l6230, 3 are constant and 3 are PWM. This signals goes to logical gate on driver. If I want to work with 6 MOS instead of l6230, how can I have 6 signals (U_low, U_hig, V_low,....) thank you2012-10-30 8:12 AM
Hello,
If I define enable (with steval ifn003v1, this params are off) the following settings in file ''Drive parameters.h'' like this, #define HIGH_SIDE_IDLE_STATE TURN_ON #define LOW_SIDE_IDLE_STATE TURN_ON the logic signals output from stm32 will be able to control directly the MOS ?. The goal of this post is to test the stm32 with an other driver than L6230 ( here, directly 6 MOS) Thank you,2012-11-08 9:00 AM