Posted on August 03, 2012 at 04:44i am using the F0 DISCOVERY, after down load my build, when i want to down load again,the ST-LINK reports 'no target connected ', i reinstalld the driver, but it is not useful, what should i do
Posted on August 08, 2012 at 09:34now the F0 DISCOVERY can enter the BOOT0 MODE, I download the UART tool ' Flash_Loader_Demonstrator_v2.5.0', it can read the IC ,but it seem can't support it
Posted on August 04, 2012 at 03:12i try to get the board into BOOT mode,was my steps wrong?1 remove R26, then 10 KOhm pull-up resistor to solder R272 fit the SB14 SB15, then press 'download'button,but the same wrongwhat should i do next(i using k...