Posted on May 17, 2011 at 12:45hi , i have to use two adc channels , one is used to measure the temperature that channel is adc channel 17, and other channel is adc 14 for other purpose. channel 17 is internal channel ,by sending adc count on UART i...
Posted on May 17, 2011 at 12:45hi Friends, i have to used two adc channels , one is used to measure the temperature that channel is adc channel 17, and other channel is adc 14 for other purpose. channel 17 is internal channel , i can see its adc cou...
Posted on May 17, 2011 at 12:42hi , i want to transmit data only with spi, not to receive in stm32f103xx how to do it ? plz give an idea!! thanks, [ This message was edited by: mayurr on 18-08-2008 13:20 ]
Posted on May 17, 2011 at 12:42hi Friends, I have to generate an timer interupt after every 0.005 ms for tim2 in stm32f103xx. and i have to on LED for 5 second and off it for 5 second . in practical case LED ramain on for 2 second and remain off for...
Posted on May 17, 2011 at 12:41 sir, I have to generate 0.005 ms tim2 interupt for stm32f103xx. and i have to on -off LED after every 5s . but it is not haappenibng in practical case. in practical case LED on-off very fast near about after every 2 s...