2008-08-18 05:23 AM
timer interupt ----please help for TIM2 in stm32F103xx
2011-05-17 03:42 AM
hi Friends,
I have to generate an timer interupt after every 0.005 ms for tim2 in stm32f103xx. and i have to on LED for 5 second and off it for 5 second . in practical case LED ramain on for 2 second and remain off for 2 second . can anyone give an idea where am i wrong? why LED is not on for 5 second and not off for 5 second . is there any setting in TIM2 ? my program : GPIO_InitTypeDef GPIO_InitStructure; NVIC_InitTypeDef NVIC_InitStructure; TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure; #ifdef DEBUG debug(); #endif /* Configure the system clocks */ RCC_Configuration(); /* NVIC Configuration */ //NVIC_Configuration(); /* Configure PC0,PC1,PC2,PC3 output push-pull */ GPIO_DeInit(GPIOC); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0; //| GPIO_Pin_1| GPIO_Pin_2; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_Init(GPIOC, &GPIO_InitStructure); // PORT C as output NVIC_DeInit(); NVIC_InitStructure.NVIC_IRQChannel = TIM2_IRQChannel; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =2; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0x00; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); /* Time base configuration */ TIM_DeInit(TIM2); TIM_TimeBaseStructure.TIM_Period =0xFFFF; TIM_TimeBaseStructure.TIM_Prescaler =0x02; TIM_TimeBaseStructure.TIM_ClockDivision = TIM_CKD_DIV1; TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up; TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure); /* Clear TIM2 update pending flag */ TIM_ClearFlag(TIM2, TIM_FLAG_Update); /* TIM IT enable */ TIM_ITConfig(TIM2, TIM_IT_Update, ENABLE); /* TIM2 enable counter */ TIM_Cmd(TIM2, ENABLE); while (1) { } } //interupt timer routine: void TIM2_IRQHandler(void) { static unsigned long Timer_Value=0; if(Flag==0) { GPIO_SetBits(GPIOC,GPIO_Pin_0); if(++Timer_Value==1000000) { Timer_Value=0; Flag=1; } } else { GPIO_ResetBits(GPIOC,GPIO_Pin_0); if(++Timer_Value==1000000) { Timer_Value=0; Flag=0; } } }2011-05-17 03:42 AM
Hi mayurr,
Note that TIM2CLK is equal to APB1 Clock If (APB1 prescaler =1) else it is APB1 Clock x2 : refer to RM0008 rev5 on web (Figure 8), You can also refer to STM32F10xFWLib_v2.0.2/FWLib/examples/TIM/TimeBase example that you can find on webhttp://www.st.com/stonline/products/support/micro/files/um0427.zip
Hope this helps you. Cheers, STOne-32.