Posted on January 24, 2012 at 08:01Hi We want to overclock the L6470 (10MHz instead of 8MHz at OSCIN) to increase maximum RPM. The resolution will be reduced, this is clear, but is there any other risk to do so? Regards Michael
Posted on December 22, 2011 at 15:03HiWe have measured the output signals of the bridges in 1/128 and 1/32 step mode and we can’t see a different voltage resolution between these 2 modes (see attachment). We have used the “GoTo�-command for th...
Posted on December 06, 2011 at 08:58HelloWe’re currently testing the possibility of using the L6470. It’s working well in full rotation with using the “Run�-command. Additional, we want to perform a ±pos mode with intermediate points and a ...
Posted on January 24, 2012 at 07:28Hi Encrico, Yes, meanwhile I came to the same result; I have calculated it, and it fits to the measuring values. Is the maximum value (255) equal to 100% KVAL or is there any additional reserve? Regards Michael
Posted on December 22, 2011 at 14:22Dear Enrico,Thanks for your comment. I will try it with the SNYC-signal. It’s a little bit contrary to our plan to delegate more control jobs to the driver, but if there is no other solution…Best Regards Michael