cancel
Showing results for 
Search instead for 
Did you mean: 

L6470: Overclocking?

michaelkroneberger9
Associate II
Posted on January 24, 2012 at 08:01

Hi

We want to overclock the L6470 (10MHz instead of 8MHz at OSCIN) to increase maximum RPM. The resolution will be reduced, this is clear, but is there any other risk to do so?

Regards

Michael
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Enrico Poli
ST Employee
Posted on January 25, 2012 at 14:22

Dear Michael,

The system clock is used by the L6470H to generates many timings and some of them are critically related to the device safe operation.

The device is designed to be robust and small variations from nominal value are tolerated, but a variation of 25% exceeds the limit.

Kind Regards

Enrico