Thanks Markus!I tested further and found that if I hand-edit the .ioc file and change the rev from 1.14.0 to 1.13.0, then it will use the older package.I should mention that the entire reason I've gone down this path is because I had actually modifie...
New CubeIDE question....I just tried STM32CubeIDE for the first time, install on Fedora 27 via the RPM install. Smooth install, no problems--nice!I'm using the STM32L452RE board, and I wanted to use the 1.13.0 libraries I had been using on my pro...