cancel
Showing results for 
Search instead for 
Did you mean: 

Sending Junk 128 bytes during Double Buffering

sivakumar4312
Associate II
Posted on September 06, 2010 at 13:35

Sending Junk 128 bytes during Double Buffering

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ashley23
Associate II
Posted on May 17, 2011 at 14:05

Double buffering is a nightmare due to the basic documentation and examples provided.  I use the code below and get no junk through...

        // Initialize Endpoint 1 double buffered bulk IN (device tx)

        SetEPType(ENDP1, EP_BULK);

        SetEPDoubleBuff(ENDP1);

        SetEPDblBuffAddr(ENDP1, ENDP1_TXADDR0, ENDP1_TXADDR1);

        SetEPDblBuffCount(ENDP1, EP_DBUF_IN, Device_Property.MaxPacketSize);

        ClearDTOG_TX(ENDP1);    // Clear DTOG

        ClearDTOG_RX(ENDP1);    // Clear SW_BUF - Sets buf 0 as software buffer and no buffer for USB peripheral

        SetEPTxStatus(ENDP1, EP_TX_NAK);

        SetEPRxStatus(ENDP1, EP_RX_DIS);

        

        // Initialize Endpoint 2 double buffered bulk OUT (device rx)

        SetEPType(ENDP2, EP_BULK);

        SetEPDoubleBuff(ENDP2);

        SetEPDblBuffAddr(ENDP2, ENDP2_RXADDR0, ENDP2_RXADDR1);

        SetEPDblBuffCount(ENDP2, EP_DBUF_OUT, Device_Property.MaxPacketSize);

        ClearDTOG_RX(ENDP2);    // Clear DTOG

        ClearDTOG_TX(ENDP2);    // Clear SW_BUF

        ToggleDTOG_TX(ENDP2);   // Toggle SW_BUF - Sets buf 1 as software buffer (buf 0 for first rx)

        SetEPRxStatus(ENDP2, EP_RX_VALID);

        SetEPTxStatus(ENDP2, EP_TX_DIS);

        

sivakumar4312
Associate II
Posted on May 17, 2011 at 14:05

Thanks Duncan,

I have already tried the code which u have sent , then the problem which i am facing is...

In the reset i used the code which u have sent, and in my send function after toggling(DTOG_RX)  i used the  SetEPTxStatus(ENDP3, EP_TX_VALID); to send the data to the host, but even at that time for the first time i am getting junk data.

Thats why i moved the  SetEPTxStatus(ENDP3, EP_TX_VALID);  to the USB_reset function and trying.

Please send me the code snippet that your are using for sending, i will cross check.

Thanks

Siva