Hello, I found another product example for some references of components, with your STM32 MCU part number, integrating a SMPS : this is a Nucleo-64 kit based on MB1841 board , you can access to documentations here :NUCLEO-U545RE-Q - STM32 Nucleo-64 d...
Hello @ Amol1,The IBIS model is available on this page here : M95020-W - 2 Kbit SPI bus EEPROM with high-speed clock - STMicroelectronics, IBIS Models, just click on the "Load more" arrow, you can access to https://www.st.com/resource/en/ibis_model/...
Hello @omarmalk , I think we do not proceed to schematics reviews on the forum. Nevertheless, if you have doubts about your power configuration, please take a look at the AN5373 which describes the configuration with SMPS (see chapters 2.2 and 8.2 fo...
Hello @walterg,In addition to the STM32L4R9I EVAL Board, there is the STM32L4R9I-DISCO (32L4R9IDISCOVERY), which embeds a DSI Connector (with default round LCD display 1.2" of 390x390 pixels ) and also embeds a DCMI connector interface compatible wit...
Hi @LCE ,I understand. In that case, one may have to wait the availability of Spice model in the CAD ressources folder of main Web page (or ask for it to the online support accessible at the ST support & Community / Support page).In parallel, please ...