Posted on May 17, 2011 at 13:37Hi, Can anyone in the forum guide me to the access speed for the on board FLASH of the STM32F103RBT6 device? Also has anyone done any benchmarking for the interrupt latency time for the following cases: 1. Interrupt Ha...
Posted on May 17, 2011 at 13:35Hi JJ, Thanks for the response. Please see the response to some of the questions: 1. Can you replicate this issue on a 2nd (or better still several) other boards? (strength in numbers) [RSM] We are expecting some new h...
Posted on May 17, 2011 at 13:35Hi, This is a follow up to my previous posting. I took some measurements on the Scope to understand how the bits are being shifted out on the MISO pin when the STM32 SPI is configured as a Slave in Full Duplex Mode. I ...
Posted on May 17, 2011 at 13:35Hi, I’m trying to use the SPI1 on STM32F103RBT6 device and have some issues. The SPI1 is configured as a slave in full duplex mode and the NSS is controlled by the Master which is another ARM processor. In the test tha...