Hi Robert,Thanks for sharing your analysis.BAT30F4 (0201 package) presents a higher leakage current at 5V (simulation = 50µA at 60°C) than other diodes suggested on the datasheet.In 0201 package, we propose : NSR01L30NXT5G that presents a low current...
Hi Matteverze, A functional and fully protected schematic is below. TCPP01-M12 :BD presentation on CC lines for type-C6V OVP on VBUS with associated load switch STL6N3LLH6 to protect against defective adapterECMF2-40A100N6 for data-lines :ESD 8kVCMF ...
Hi, Thanks for sharing your case. You are looking for basic Type-C SINK with 1.5A max without Power Delivery (STM32U0 series). Legacy current on USB-C VBUS is 5V 0.5A when VBUS turns-on.The system must be able to start below this current threshold. ...
Hello, Using, external OCP (high side amplifier + comparator) will be more expensive (and complicated) than on the shelf integrated solution.Both solutions can drive VBUS load switch (MOSFET used to activate VBUS) to perform OCP. Use TCPP03-M20 for ...
Hello, Thanks for your question ! TCPP01-M12 has been tailored to optimize cost then it embeds only key protections for SINK (OVP on VBUS / CC + ESD). When VBUS OCP is needed, TCPP03-M20 can perform SINK only solution with OCP feature. It is the reco...