Posted on May 17, 2011 at 13:35Hi! I`ve found bug in StdPeriph library version 3.1.2. Function ADC_InjectedChannelConfig is incorrect configuring ADC_JSQR register. In stm32f10x_adc.c line 974 must tmpreg2 = JSQR_JSQ_Set << (5 * (uint8_t)((Rank + 1)...
Posted on May 17, 2011 at 13:31Unfortunately I have no possible to try with other boards. I check PCB many times - there is ok. Do you can test STM32CBT6 device for this and report me for result. May be only my chip is corrupt...
Posted on May 17, 2011 at 13:31Hello! -On PC side I use (um0462) Flash loader demonstrator v2.0 -When PB0 is low, I can`t connect to device through USART, but if PB0 is open circuit connection is successful. -PB0 using as input (normally pulled down...