Posted on May 17, 2011 at 13:21aaaah thx! in the datasheet, not in the manual, there is a big table of all pins with all alternate functions and remaps of all packages
Posted on May 17, 2011 at 13:21Hi, where i can find the GPIO mapping of the SPI2 (64/100 or 144 pin devices)?? I think the description of a lot of alternate pin functions are missing in the manuals...(e.g. SPI2) ??
Posted on May 17, 2011 at 13:20Hi, is it possible to start a DMA transaction by a falling edge on a GPIO pin (STM32F103CB)? I used the EXTI configuration for this input pin and in the EXTI-ISR i can trigger the DMA. But i think this is not a really ...