2009-08-06 6:02 AM
DMA-trigger via GPIO-pin
2011-05-17 4:20 AM
Hi,
is it possible to start a DMA transaction by a falling edge on a GPIO pin (STM32F103CB)? I used the EXTI configuration for this input pin and in the EXTI-ISR i can trigger the DMA. But i think this is not a really good solution, because of a trigger-signal of 9 - 18 MHz. So i want to trigger the DMA by the hardware. Greetings Hirbel