Posted on May 17, 2011 at 13:23Hi edison, Thanks for the reply and excuse me for not answering soon, but things evolved a little. I can now successfully launch my application, both from the AN2557 IAP and from my own bootloader. The problem was that...
Posted on May 17, 2011 at 13:23One update and some apologies. The bootloader successfully jumps to my application, which start correctly but it seems to do nothing because the systick irq is not triggering. I made another build which does not use th...
Posted on May 17, 2011 at 13:23Hi all. I'm having troubles in starting my application downloaded with the UART IAP (AN2557) All is well if I build the example project and download it, but nothing works if I build my own project: download is ok but t...
Posted on May 17, 2011 at 13:22Hi Andreas, 1) NVIC_SystemReset I have the same problem with a new Ulink2 on two different samples of Keil MCBSTM32 and one STM32F120X-128K-EVAL boards... 2) IWDG does not reset during debug (seems ok wehen Jtag not co...
Posted on May 17, 2011 at 13:22Hi all, I posted this a mounth ago but nobody answered. I still have the same problem and I'm seriously considering switching to another microcontrolloer/environment. I'm using the keil MCBSTM32 demoboard (F103RB micro...