Posted on May 17, 2011 at 13:20Hi folks, im trying to get the the stm32 to sample at 1M Samples/sec but only getting max the half .... what is wrong ??? I use Timer1 and DMA to trigger Ad converter. The timer is triggering at 1MHz in this config. I ...
Posted on May 17, 2011 at 13:17Hi folks, Has anybody worked with stepper motor on stm32 ?? I have seen the appnote with the L6208, but it's expensive, and i dont need microstepping ..... best reg. Finn