Posted on May 17, 2011 at 09:58Hi all, In the pdf document called Application note AN2475 (page 8) ST wrote. ST provides a free Flash loader utility allowing the program of the STR91xFA internal Flash Bank0 using an IAP driver to be loaded in the Fl...
Posted on May 17, 2011 at 09:58Hi Does anyone here have succes with the bootloader AN 2475 IAP example, using the Hyperterminal?. I'm searching for someone who can help me with a modifyed example that works correct. If some one here have the source ...
Posted on May 17, 2011 at 09:58Hi, Well, I have modifyed the 91x_init.s to : #define Flash_512KB_Bank1_Boot + the flash loader is the one for 1_2MB products -->you have to change it to be for 256K/512KB products (the default one) Can you please spec...
Posted on May 17, 2011 at 09:58Hi, Does ANYONE here have a succesfully boot loader IAP running with an UART interface ( AN2475 ). If anyone have a sucessfully IAP example ( AN2475 ) running then I'm very interested to get/see this code, because I ha...