Posted on May 17, 2011 at 11:32hi everybody, can anyone who worked with AD7490 can send the sample code.its urgent.im trying to interface it with STR912. anyone plz help me out as soon as possible. thankx in advance regards madhu
Posted on May 17, 2011 at 11:321)By configuring the PWR bit in the RTC_CR register, you can select to power only the RTC or both the RTC and the SRAM from VBATT. 2)Have u Selected the Option mentioned above,if so see if u are modifying the RTC CONTR...
Posted on May 17, 2011 at 09:58hi, iam trying to interface str912 to ADC7490 using SSP. which one we can use as a master/slave either adc/controller. my SSP configuration seems like SSP0->CR0 = 0x0487; //Serial CLK Rate(SCR) 4,Motorola,SCLK held l...