Posted on May 17, 2011 at 13:29Has anyone flashed an STM32 using the ARM RVDS tools? We are attempting to use ARM RVDS 4.0 for a new STM32 project and are unable to get a board to flash. We can connect to the board and download to RAM with out any i...
Posted on May 17, 2011 at 12:46GHS support is very good. I am currently using Rowley for development on the STM32, but I did setup a project with my GHS tools orginally. I was using Multi 5.0.3 and needed to upgrade the firmware in my GHS probe to s...
Posted on May 17, 2011 at 12:42Hi jrubis, STM32 is embedding (ARM Cortex-M3 Core) that performs 1.25 DMIPS/MHz (Dhrystone 2.1) out of flash at 0 wait state. Coldfire V2 performs 0.9 DMIPS/MHz (Dhrystone 2.1) I thought at 72 MHz you must insert 2 wa...
Posted on May 17, 2011 at 12:25I also ported over the EVB Demo Program and have it running now. Since this is a rather large program, with lots of functions, I figured it would be a good test.