2009-02-25 5:04 AM
IAR optimiser
2011-05-17 4:04 AM
When you select: no optimization, do you have the same problem?
2011-05-17 4:04 AM
Hello. Im using IAR 5.3 kickstart version and processor STM32F10xx4 with the optimiser FULL and on speed. When I use #define to remove part of my code with #ifdef ....#endif, the part inside is not skipped even if #define is uncommented. Please, did anyone meet a similar situation? For the time being I will use normal comments. Thanks Johann
2011-05-17 4:04 AM
Hello M3allem. Hope you are fine. No I do not get this problem. Thanks. Nice evening.
2011-05-17 4:04 AM
can you share your code?
2011-05-17 4:04 AM
M3allem hit it right on the nose.
You may wish to experiment by turning minimal optimizations ON - and noting ''if/how'' they effect compilation. You can then continue this process - and discover ''just when'' you run into trouble. Then you can decide if you want to ''quiet'' the error (modify your code) or accept the less than optimal compilation...