Posted on May 17, 2011 at 09:50Hi Ollos, Here is a copy of the message I sent to Adam's mailing list in Sweden. Did you have to deal with the issues of the dabort_handler trapping exceptions from the IAR implementation? -Bill I am attempting to use ...
Posted on May 17, 2011 at 09:50Hi Ollos, I spoke with Paul Curtis at Rowley some time ago and he indicated they are developing their own stack. Not sure where he is in this process, but you might want to email him. I also have a project which requir...
Posted on May 17, 2011 at 09:50I found the answer on Rowley's website: With a lot of ARM CPUs it is not possible for the debugger to reset the target and maintain control of it over the JTAG interface, this means that a program will run for a period...
Posted on May 17, 2011 at 09:50Apparently this needs to be set somewhere in the dev environment (I am using Rowley CW), but I cannot find any reference to this switch or where it should be set (or even what it does). Anyone out there able to help? -...
Posted on May 17, 2011 at 09:50has anyone run the example successfully for the I2C on the eval board? I connected P2.0->P2.2 and P2.1->P2.3 and used 1K pullups to 3.3VDC. I run the code and when I look with my scope on the clock line, it transitions...