cancel
Showing results for 
Search instead for 
Did you mean: 

I2C on STR910-Eval board

williamjsell
Associate II
Posted on February 25, 2008 at 14:53

I2C on STR910-Eval board

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
williamjsell
Associate II
Posted on May 17, 2011 at 09:50

has anyone run the example successfully for the I2C on the eval board? I connected P2.0->P2.2 and P2.1->P2.3 and used 1K pullups to 3.3VDC. I run the code and when I look with my scope on the clock line, it transitions from high to low and stays there. The interrupts never bang off, so no data is transmitted. Not sure how to even debug this, given I using ST-developed sample code. Any ideas?

-Bill