Posted on May 17, 2011 at 12:26I used this ftoa fun it doesnt working. same function was working in PC version compiler is there any options to add for floating point operations? i also add the options like -mfpu=vfp -mfloat-abi-softfp but it also ...
Posted on May 17, 2011 at 12:26Hi, I use stm32.ld in stm32fwlib folder. what to do resolve the size and how to use c printf functions using that examples ? is there any procedure to add more linking and compile options? can any one help me ?
Posted on May 17, 2011 at 12:26Hi, i use codesourcery g++ lite. i used ld - T generic.hosted.ld stm32.ld i got main.bin file size more in MBs.I want use sprintf ,printf function. what is the procedure to do ld? following files size: Volume in drive...