Posted on May 17, 2011 at 13:23Hi @all, I have a problem with the RTC Alarm Interrupt in combination with the Stop mode and do not come to a solution. Can please somebody help me here. My application has to wake up in 60s intervals and check if it h...
Posted on May 17, 2011 at 12:17Hi, can the Vrefint Channel be used as the Reference for AD12? Or is the only Reference Voltage the Vref+/Vref- Pin? Thanks, Joachim
Posted on May 17, 2011 at 12:16Hello STOne-32, is it possible to give exacter time designation? First Quarter, second quarter ...? Are they pin compatible with the 128k devices? Thanks, Joachim
Posted on May 17, 2011 at 12:16Hello, the STM32 would be a great solution for our project. But we need at least 256kb flash and 20kb ram. When will devices with more memory available? Thanks in advance, Joachim Stümpfl