cancel
Showing results for 
Search instead for 
Did you mean: 

Devices with more memory

jstuempfl9
Associate II
Posted on October 25, 2007 at 09:23

Devices with more memory

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
jstuempfl9
Associate II
Posted on May 17, 2011 at 12:16

Hello,

the STM32 would be a great solution for our project. But we need at least 256kb flash and 20kb ram. When will devices with more memory available?

Thanks in advance,

Joachim Stümpfl

16-32micros
Associate III
Posted on May 17, 2011 at 12:16

Dear Joachim,

Future family of the STM32F103xx performance line is growing and will see an expansion of the current options. Larger packages will soon be

(Next Year ;-)), available with up to 512KB Flash, 64KB SRAM and with extended features such as EMI support, SDIO, I2S, DAC and additional timers and USARTS.

You can start your design evaluation from Now, using the 128K Flash and playing with this platform to be familiar with the Features until the 256K of Flash ( and more) is ready for your production :) next year.

Regards, STOne-32

jstuempfl9
Associate II
Posted on May 17, 2011 at 12:16

Hello STOne-32,

is it possible to give exacter time designation? First Quarter, second quarter ...? Are they pin compatible with the 128k devices?

Thanks,

Joachim

jstuempfl9
Associate II
Posted on May 17, 2011 at 12:16

Thanks a lot.

Joachim

whennes
Associate
Posted on May 17, 2011 at 12:16

Hello Mr. Stümpfl,

samples for the 256k and 512k Flash devices are scheduled Q1/08, massproduction is scheduled Q2/08.

Best regards

Winfried Hennes

Line Development Manager ST Microelectronics

CAT - Center of Advanced Technologies

____________________________________________________

SPOERLE - A Division of Arrow Central Europe

Arrow Central Europe GmbH

Max-Planck-Str. 1-3

D-63303 Dreieich

Ph. +49 (0)6103/304-8200 Mob. +49 (0)15116242046

Fax +49 (0)6103/304-118200

mailto:whennes@spoerle.com

http://www.spoerle.de

[ This message was edited by: WHennes on 25-10-2007 10:46 ]