Posted on May 17, 2011 at 10:14I also have a question about how to measure the current consumed by the motor. I have tried measuring it at jumper w6, but am not able to get a clear reading. Is there a test point on the development kit where you can ...
Posted on May 17, 2011 at 10:14Hi, I have a similar question to last time! I am now trying to use a sinusoidal input on the same motor (1 pole pair, closed loop, with 1 hall sensor connected). The maximum speed I can run the motor at without it gett...
Posted on May 17, 2011 at 10:14Hi gforte, Thanks again for your help! I will see if 40800RPM is fast enough, and will try modifying the settings if it's not. I'll let you know how it goes. Thanks so much! Kel
Posted on May 17, 2011 at 10:14Hi Gigi, Thanks for your help. I have a motor with only 1 pole pair. So it looks like the maximum RPM = 680Hz * 60 / 1 = 40800 (is there any way to increase this?) Hopefully this will be sufficient! Thanks again! Kel
Posted on May 17, 2011 at 10:14Hi! I am trying to run a 29v BLDC motor at 50,000rpm in either open or closed loop mode. I have read the threads relating to maximum speeds, and also application notes. However, I am still a little confused about how t...