cancel
Showing results for 
Search instead for 
Did you mean: 

Max RPM for a PMAC motor

poole
Associate II
Posted on June 01, 2007 at 05:04

Max RPM for a PMAC motor

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
poole
Associate II
Posted on May 17, 2011 at 10:14

Hi,

I have a similar question to last time! I am now trying to use a sinusoidal input on the same motor (1 pole pair, closed loop, with 1 hall sensor connected).

The maximum speed I can run the motor at without it getting really hot is about 15000RPM. Is there any way I can increase this without increasing the current consumption?

Thanks!!

Kel

poole
Associate II
Posted on May 17, 2011 at 10:14

I also have a question about how to measure the current consumed by the motor. I have tried measuring it at jumper w6, but am not able to get a clear reading. Is there a test point on the development kit where you can measure the current?

(I am sorry for this question - I realise it is a dumb one!!)

Thanks heaps!

Kel