Posted on May 17, 2011 at 09:40Hello, I will give more informations so you can help me , the STR9 I am using is the STR912FZ44H6 (BGA) but this reference doesn't exist neither in CAPS 2.40 and the JTAG Programmer 1.20, so I choose the STR912FAZ44H6,...
Posted on May 17, 2011 at 09:40Hi, when I try to flash the STR9 with CAPS 2.40 I get an error message when programing configuration, I also have difficulties downloading firmware with IAR 4.40A. I am using the STR912FAZ44H6 (BGA), before I was using...
Posted on May 17, 2011 at 09:39Hello, I am using the UART0 in interrupt mode , the problem is that after sending the last byte and clearing the pending interrupt the Tx interrupt still occurs ( i am not using break mode ), I want to know how to stop...