Posted on May 17, 2011 at 12:15But I just don't trust Luminary to be alive in 10 yearsWhat model of crystal ball are you using? Perhaps you could download a new firmware for it? :-) I have datasheet for STR720RBQ6, but it is not in ST portfolio. Any...
Posted on May 17, 2011 at 09:45You should replace GPIO_IPConnected_Enable by GPIO_IPConnected_DisableWhat does the IP stands for? I found no explanation of it in the documentation. Would you please explain it? Thank you.
Posted on May 17, 2011 at 09:44Perhaps I was not very clear, when I say ignore the first byte back :-[ Obviously you need to transmit 0xff after the command, until you have clocked in the required amount of bytes. In all instances I have seen the f...
Posted on May 17, 2011 at 09:44Basically you can always ignore the first byte back from the SD card, as all commands needs at least one byte, and you will probably find the second byte is 0x01.I am not sure what you mean by ''ignore the first byte''...
Posted on May 17, 2011 at 09:44The problem I have is that I can see on the scope that the Chip Select(nss)goes high after every byte sent, and then the SD Card does not respond correctly if that happens.It is easier to de-couple the CS from the rest...