Posted on June 22, 2006 at 13:39hello, i have an problem with my RX_TX_Interrupt. i am trying to write data toward an I2C slave. The procedure is the following: 1. i initialise my I2c with the ITE bit set 2. my task send a Start condition 3. the in...
Posted on May 17, 2006 at 08:57Hi, I did multiple tests and I do not understand what I notice. First of all, my str710 have a frequency of 48 MHz. First test =========== I plug a frequency generatior on a GPIO0/bit10. I bind an handler itxti() on th...
Posted on May 09, 2006 at 06:19hello, i would like to configure the P1.11 as external interrupt. how do you it? It is possible to show me what register are configured to use correctly this pin. thanks Ludovic
Posted on May 04, 2006 at 13:21I am working on a project where there is a pushbutton. My question is : Is possible to use the can pin to produce the pushbutton interrrupt? because the other External interrupt(XTI)pin are used for other device. Or Do...
Posted on May 02, 2006 at 05:54hello, thanks for your answer. the problem has been resolved.: at the output of the TIM1 a component( transistor) inverse the signal. now i play an wav file with th TIM1 at 8Khz frequency but have a correct sound but i...