cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt latency and cpu clock

ludo98
Associate II
Posted on May 18, 2006 at 14:09

Interrupt latency and cpu clock

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ludo98
Associate II
Posted on May 17, 2006 at 08:57

Hi,

I did multiple tests and I do not understand what I notice.

First of all, my str710 have a frequency of 48 MHz.

First test

===========

I plug a frequency generatior on a GPIO0/bit10.

I bind an handler itxti() on that interrupt, call by XTI_IRQHandler()

The handler generate a pulse on each interrupt.

Then, I watch the result on a oscilloscope and I notice a latency between the clock and the pulse of 15 micro secondes.

__arm void XTI_IRQHandler(void)

{

register unsigned int b=0x01; /* bigger than u8 because of condition stop i<=128 */

register unsigned int i=0;

register unsigned char h = XTI->PRH&=XTI->MRH;

register unsigned char l = XTI->PRL&=XTI->MRL;

while ( (h || l) && b<=128) {

if (h & b ) {

(XTI_handler[i+0x8])(EICXTI_data[i+0x8+32]); // test_itxti is called here

XTI->PRH &= ~b;

h &= ~b;

}

if (l & b ) {

(XTI_handler[i])(EICXTI_data[i+32]);

XTI->PRL &= ~b;

l &= ~b;

}

b<<=1;

i++;

}

}

static void test_itxti(void*d) {

XTI_PendingBitClear(XTI_Line13);

//WRITEIO(RST_CODEC,0);

//GPIO_BitWrite(GPIO0, 7,0);

for (int i=0;i

WRITEIO(RST_CODEC,1);

}

Second test:

============

I did almost the same thing except I write on the IO in the function XTI_IRQHandler()

Then I notice a latency of 7 micro secondes.

__arm void XTI_IRQHandler(void)

{

register unsigned int b=0x01; /* bigger than u8 because of condition stop i<=128 */

register unsigned int i=0;

register unsigned char h = XTI->PRH&=XTI->MRH;

register unsigned char l = XTI->PRL&=XTI->MRL;

GPIO_BitWrite(GPIO0, 7,0); //<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<<

while ( (h || l) && b<=128) {

if (h & b ) {

(XTI_handler[i+0x8])(EICXTI_data[i+0x8+32]); // test_itxti is called here

XTI->PRH &= ~b;

h &= ~b;

}

if (l & b ) {

(XTI_handler[i])(EICXTI_data[i+32]);

XTI->PRL &= ~b;

l &= ~b;

}

b<<=1;

i++;

}

}

Third test :

============

I generate the pulse directly in the IRQHandler(71x_vect.s79).

I notice a latency of 2 micro secondes

addr DCD 0xE000300C

IRQHandler

SUB LR,LR,#4 ; adj for proper CMX return

STMFD SP!,{R0-R12,LR} ; save the registers

MRS R9,SPSR ; save the SPSR

STMFD SP!,{R9}

; TEST IT

LDR R0, addr

LDRH R3,[R0]

mov r4,#0x80

bic R3,R3,R4

STRH R3,[R0]

; end

...

Finaly, I did this test :

IRQHandler

SUB LR,LR,#4 ; adj for proper CMX return

STMFD SP!,{R0-R12,LR} ; save the registers

MRS R9,SPSR ; save the SPSR

STMFD SP!,{R9}

; LUDO TEST IT

LDR R0, addr1

LDRH R3,[R0]

mov r4,#0x80

ORR R3,R3,R4

STRH R3,[R0]

LDR R0, addr2

LDRH R3,[R0]

BIC R3,R3,R4

STRH R3,[R0]

LDR R0, addr3

LDRH R3,[R0]

ORR R3,R3,R4

STRH R3,[R0]

LDR R0, addr

LDRH R3,[R0]

mov r4,#0x80

DEB:

bic R3,R3,R4

STRH R3,[R0]

NOP

NOP

NOP

NOP

NOP

NOP

NOP

NOP

NOP

ORR R3,R3,R4

STRH R3,[R0]

NOP

NOP

NOP

NOP

NOP

NOP

NOP

NOP

NOP

B DEB

; LUDO

Then I see a sqare signal of .68 micro seconde period.

0.68.10^-6 / 24 instructions = 0.28.10^-7

freq = 1/0.28.10^-7 = 35 MHz

Conclusion :

I lose time when I execute simple instruction ?

I do not understand why I need 15 micro secondes to call a handler ?

15uS = 525 instructions at 35 MHz.

7uS = 250 instuctions

I think I need only 50 instructions to get in the XTI_IRQHandler() ?

Do you understand my questions ?

Did I make mistakes in my tests ?

What do you suspect ?

Thanks for your help.