Posted on May 17, 2011 at 15:07Ciao Etaphi , My idea is to use an hardware timer(like tim4) as free running counter by resetting its counter on the first interrupt,and read the counter value (and reset it again) on the next interrupt. Do you agree...
Posted on May 17, 2011 at 15:07Hi,I have an hard question. I have an external interrupt generated by the power line (50hz). I'm using an stm8s and I'm using the STM8S207RBT6 and the pin PE6 for the external interrupt. All hardware timers are availab...
Posted on May 17, 2011 at 15:05Dear brazov2, I didn't understand your answer.I know that I can check the reset source but I have mentioned the emc application note only because I have read on it the illegal op-codes list. I agree with you that if th...