cancel
Showing results for 
Search instead for 
Did you mean: 

Trials with ST7LITEU09M6 mcu and ad converters

epassoni9
Associate II
Posted on December 10, 2009 at 12:18

Trials with ST7LITEU09M6 mcu and ad converters

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
epassoni9
Associate II
Posted on December 10, 2009 at 12:18

Hi,

I'm doing some trials with an st7liteu09m6 and its ad-converters.

I'm using the internal resonator with an fpu equal to 4mhz.

The adc conversion speed is equal to fpu/2,so 2 mhz.

I have connected a 10k resistor between one of the adc input pin

of the mcu on one side and to the ground the other side.

The problem is that I see about 20mv between the input pin and the resistor when I expect to see about 0 Volts.(It seems a voltage generated by the adc input pin).

What it can be ?

best regards

Spectre

http://picpaste.com/pic.JPG

http://picpaste.com/pic.JPG

(take a look at the link because the image tag seems to be not working)