Posted on September 18, 2006 at 05:54Hi, In STR71xLib (rtc.h) the 32 bit RTC counter is read with two consecutive 16 bit reads. Isn't there a risk that the counter changes between theese two reads? /Johnny
Posted on May 02, 2006 at 10:54In the datasheet for STR712 it says that you can program data flash 100 000 times. My question is, does a programming (without erase) of 0xFFFFFFFF also decrease no of endurance cycles. Regards Johnny
Posted on April 07, 2006 at 10:54Hello, I am sending data on BSP1 and check the TUFL bit to see when transmission is finished. The problem is that TUFL will not get set. Are there any special considerations regarding this bit? I thought it got set w...