cancel
Showing results for 
Search instead for 
Did you mean: 

Transmit underflow bit (TUFL) in BSPI

johnny
Associate II
Posted on April 07, 2006 at 11:44

Transmit underflow bit (TUFL) in BSPI

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
johnny
Associate II
Posted on April 07, 2006 at 10:54

Hello,

I am sending data on BSP1 and check the TUFL bit to see when transmission is finished. The problem is that TUFL will not get set. Are there any special considerations regarding this bit? I thought it got set whenever the transmit buffer is completely empty (no transmission and nothing in transmit buffer).

Regards

Johnny