Posted on September 05, 2006 at 09:54A note in section 2.3 (Write Operation) of STR7 Flash Programming Reference Manual says that the first write/erase operation makes flash bank0 not accessible. However, even when looking in section 2.3.3 (Memory C...
Posted on June 07, 2006 at 08:37Hi. My code is running in bank 0 and it needs to write in the same bank. This is forbidden so can I store the code that will write to bank 0 in bank 1? (for instance sector B1F0) (to avoid having to copy code in RAM a...
Posted on March 21, 2006 at 19:37Hi. Can the RTC kicks back the STR710 to life when it is in stop mode? The datasheet is not explicit about that. Thanks! Bernard
Posted on March 06, 2006 at 11:21Hi there. I'm looking for any tips to port eCos to the STR710FZ2. We still have a few weeks before getting our hands on the the first prototypes of our hardware, and I'd like to start looking at using this chip with ...