Posted on October 07, 2009 at 19:48Hi, We are about to make a production of 2000-2500 devices using STR712. Usually we upload firmware using a PC and JTAG programmer. To test our devices, we have our own testing device, which also has a STR712. We w...
Posted on July 07, 2009 at 17:20Hi, I am following AN2119 to install uClinux on str710 board. However I am not using the evaluation board, but my own board. Fortunately, it also has an external flash and SRAM on EMI, on same position/address the eva...
Posted on November 03, 2008 at 15:36Hi, I made the following test. I took a 14.756 Mhz board, which was already programmed by PC2, so it stopped working. Then, I changed the 14.756 oscillator, placing a 4 Mhz one. Now, it is working again, even in P...
Posted on November 01, 2008 at 11:54 Hi, I have the following issue: I have two PC for development, both using Rowley's CrossStudio. My boards have STR711, some with a 4Mhz and some with 756 Mhz clock. On one PC, all boards can be program...
Posted on November 01, 2007 at 12:03Well, it is strange because since I added the missing return, my application has not hanged again. It used to hang easily and frequently, but now it doesn't. Moreover, debugging with some leds, the 'hanging scope'...