cancel
Showing results for 
Search instead for 
Did you mean: 

uClinux and external memory

lgiordano2
Associate II
Posted on July 07, 2009 at 17:20

uClinux and external memory

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
lgiordano2
Associate II
Posted on July 07, 2009 at 17:20

Hi, I am following AN2119 to install uClinux on str710 board. However I am not using the evaluation board, but my own board. Fortunately, it also has an external flash and SRAM on EMI, on same position/address the evaluation board has. I have the following questions:

1) My board has no option to enable the external flash memory boot. May I write uClinux image to external flash, boot from internal memory and then ''jump'' to external? How?

2) AN2119 is based on a old kernel and uclinux version. Is there a new patch to use a newer one? I haven been able to find it.

Best regards in advance.

Leonardo