Posted on October 25, 2005 at 14:36Hi, I am using the device soldered to my application board, which is fitted with a crystal. I have selected ICP OPT Enable mode, but cannot read out from the device or reprogram the option bytes. I cannot use the I...
Posted on October 19, 2005 at 14:14 Hi, I have downloaded the latest version of the development toolset (V3.2.1) and installed it, however I am still unable to program my device. The device that I am using is a ST7FMIDI9S4T6 I am selectin...
Posted on October 13, 2005 at 10:26How can I update the list of supported devices in STVP7 to include the ST7FMIDI in order to program it using the STICK/UK programmer?