cancel
Showing results for 
Search instead for 
Did you mean: 

ST7FMIDI programming

justin2399
Associate II
Posted on February 10, 2006 at 11:14

ST7FMIDI programming

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
justin2399
Associate II
Posted on October 13, 2005 at 10:26

How can I update the list of supported devices in STVP7 to include the ST7FMIDI in order to program it using the STICK/UK programmer?

sjo
Associate II
Posted on October 17, 2005 at 08:35

Does ST have an answer on this topic, this is also of interest to me.

Regards

sjo

alain2399
Associate II
Posted on October 17, 2005 at 10:20

The ST7FMIDI-EMU3 is the name of the emulator supporting the ST72F34x familly. Those devices are officially supported from STVD7 R3.2.1 (including STVD7 and STVP7). This new release is ready for distribution and should be available soon on the WEB.

Regards,

Alain

sjo
Associate II
Posted on October 17, 2005 at 12:26

Will it be supported by the ST7STICK programmer ?

Many Thanks

sjo

alain2399
Associate II
Posted on October 18, 2005 at 14:14

STVD7 r3.2.1 is available at:

http://mcd.rou.st.com/mdtfiles/1129550622.exe

All ST tools (this includes ST7Stick programmer) supports the MIDI familly for emulation, ICD and ICP.

Enjoy

Alain

justin2399
Associate II
Posted on October 19, 2005 at 14:14

Hi,

I have downloaded the latest version of the development toolset (V3.2.1) and installed it, however I am still unable to program my device.

The device that I am using is a ST7FMIDI9S4T6

I am selecting the ST72F344x4 in the STVP tool but cannot read from or program the device using the STICK programmer.

The error message :

Error on Option Bytes (Complementary bytes). Reprogram Option Bytes of device.

appears and the process is stopped. I have attached a screen print for reference.

I have checked the hardware is OK by changing the device on the board for another (ST72F324L) and can read from and program it without problems using the STICK programmer and STVP tool.

Can anyone offer any solutions?

Cheers,

BigFella.

________________

Attachments :

option_problem.doc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I08M&d=%2Fa%2F0X0000000bU6%2FUBiyXQz1F1V1HZEEzdojPub2r7eyOrOPqHVGA.Agp1E&asPdf=false
justin2399
Associate II
Posted on October 25, 2005 at 14:36

Hi,

I am using the device soldered to my application board, which is fitted with a crystal. I have selected ICP OPT Enable mode, but cannot read out from the device or reprogram the option bytes.

I cannot use the ICP OPT Disable, since there is no connection from pin 9 (Osc) of the programming header to the micro on my board.

I do not have a ST7MDT20J socket board and so cannot try the device on its own.

Regards,

BigFella.

md1
Associate II
Posted on February 03, 2006 at 11:25

I have just downloaded the new Visual Develop 3.3.0, with Visual Develop 2.0.0.

However, the 344 support does not seem to be present?