Posted on October 28, 2005 at 18:31Greeting, If we put unused peripheral in reset state using the APBn_SWRES register, should we increase the power saving? Regards, PGagnon
Posted on October 28, 2005 at 14:30Greeting, In section 2.1.7.2 of the STR71x reference manual rev 6, a reference is made to PWD bit of the FLASH_CR0. However, the FLASH_CR0 is not documented. For future revision of the STR71x reference manual, it c...
Posted on October 14, 2005 at 18:55Greeting, I think there is an error in file pcu.h (STR71x Library Version 3.0). The PCU_LPRWFI_Mask should be defined as follow: #define PCU_LPRWFI_Mask 0x0010 The current wrong value is 0x0020. Confirmation please...