Posted on May 17, 2011 at 09:48Hi ! Source code -> see attached file. I am not working in low power mode, unless the STR9 starts per default in this mode. When I disable TIMER_IRQ it works O.K. When I enable TIMER_IRQ, I get additional UART_IRQ (RX_...
Posted on May 17, 2011 at 09:48Hi ! I use STR912FA (Revision 710) with KEIL development tools. I have a problem, when using two interrupts (Timer0 and UART0) simultaneously. Sometimes I get an spurious UART RX interrupt. I read somthing about proble...
Posted on November 13, 2006 at 11:35Hi, another hint: - when I change the file scat.scf to start the program from address 0x40000000 -> no problem But I want to use the IAP-Driver in sector 0 and so my program should be able to start at 0x40002000. ...