Posted on May 17, 2011 at 10:18Hello, I was looking at www.newyorksemi.com - they seem to have some of it left ! Best regards, Dipl.-Ing. Klaus Pelikan
Posted on May 17, 2011 at 10:18What is the MPAR register used for if DAC=1, DTE=0, PCN=0 ? i.e. Motor controller in direct access mode, only PWM U signal connected to channel manager, dead time generator disabled ! I just want to control a brushed D...
Posted on October 10, 2005 at 05:31Your are right ! In fact the TDRE Bit tells you that the transmit buffer register ist ready to be written with a new character, no matter if the actual character transmission has been completed. The TC Bit however ...
Posted on October 09, 2005 at 08:32Quote:On 09-10-2005 at 11:56, Anonymous wrote: What's the effect off the REO Bit (MPOL register) in sensorless mode - What's ment with '' BEMF Read on High channels (REO=1) or Read on Low channels (REO=0) - the edg...
Posted on October 09, 2005 at 08:26What's the effect off the REO Bit (MPOL register) in sensorless mode - What's ment with '' BEMF Read on High channels (REO=1) or Read on Low channels (REO=0) - the edge polarity is only determined by the CPB and th...