cancel
Showing results for 
Search instead for 
Did you mean: 

Problems in production with uPSD3233B

paolo_capobianco
Associate II
Posted on February 10, 2009 at 11:28

Problems in production with uPSD3233B

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
paolo_capobianco
Associate II
Posted on May 17, 2011 at 11:52

Ciao,

I'm having an increasing number of devices (uPSD3233B), which are not working properly after they've been programmed.

In particular, if I try to verify one of these devices using the FL101, I get in 80% of the times ''Unable to connect with JTAG target device'' message, and the remaining times, I'm able to start JTAG operation but immediately after I get the Error message ''device is secured''.

At the moment we are replacing these devices, but the failure rate is increasing.

Any idea?

Thanks

Paolo