cancel
Showing results for 
Search instead for 
Did you mean: 

My STPC SBC won't boot to CE desktop with Ethernet cable connected

jcrouch
Associate II
Posted on March 08, 2005 at 04:23

My STPC SBC won't boot to CE desktop with Ethernet cable connected

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jcrouch
Associate II
Posted on January 19, 2005 at 16:59

My STPC Consumer-II SBC won't boot all the way into the CE desktop if I first power up board with Ethernet cable connected. If I wait until the SBC boots into CE desktop and then connect an Ethernet cable, everything works fine. I get an IP address, and I can browse the Internet fine. I know the Ethernet cable is okay because I tested it on a nearby PC. Also, I do not have ''Boot from LAN'' enabled in the BIOS only boot from hard disk. I think that CE is trying to do something on the network before everthing related to the ethernet is loaded and configured. Therefore, it must be hanging because of this.

Thanks for any help,

Joel

anouar
Associate II
Posted on March 08, 2005 at 04:23

Hi,

Which network adapter are you using ? Which network configuration are you using? Which is the version of CE that you use ?

Tanks.