Posted on May 17, 2011 at 12:40hallo, can anybody help me. my problem is that the programming of the external flash on the stm3210e-eval is not possible. i tried to programm with DfuSe V2.2 but nothing happend. Than i found the flash loader demonstr...
Posted on May 17, 2011 at 12:39Hi @all, ich tried to run a speed codec AMR-WB on STM32F103ZE. Is there anybody who can give me an answer, if this could be possible. And perhaps is there somebody who can help me to optimize? i use the STM3210E-EVAL &...
Posted on May 17, 2011 at 12:39I use the Ansi C Code from http://www.3gpp1.org/ftp/specs/archive/26_series/26.173/ It is written as bit exakt without using of floating point numbers. (Fixed Point). I want to test the STM32 it this could be possible ...
Posted on May 17, 2011 at 12:31JP6 is fitted, an Application with WavePlayer works fine. It use Vista Business with SP1. I get an device called STM32 Speaker, but i cannot play musik on it. The standard format is 8 Bit and 22000 Hz. And it seem that...