2009-05-20 7:56 PM
STM3210B-EVAL USB Speaker Demo
2011-05-17 3:31 AM
Hallo,
i have a problem with the speaker demo application. after connecting the STM3210B-EVAL the driver is installed and a device STM32 Speaker is visible. But i can't play sounds on it. Does anybody know why? I use STM3210B-EVAL with Segger J-Link and IAR Embedded Workbench 5.11..works fine.2011-05-17 3:31 AM
I tried the same example and it works fine.
Just check that the JP6:speaker (near the LCD) is fitted.2011-05-17 3:31 AM
JP6 is fitted, an Application with WavePlayer works fine. It use Vista Business with SP1. I get an device called STM32 Speaker, but i cannot play musik on it. The standard format is 8 Bit and 22000 Hz. And it seem that this is not kompatible. I also cannot send an test tone to the device. Message : Seem device not ready...
2011-05-17 3:31 AM
Did you figure out why the speaker doesn't work? I am having the same problem. Windows detected it but the speaker does not play any sound. Windows doesn't seem to allow the volume to be adjusted for the speaker.