Posted on August 13, 2004 at 08:49Hi ParveenG, I have tried with the SPI protocol with a st7lite09, as you can find in my other question, but after a byte trasmission i have 5 volt fixed at pin 3 of the port B (used for the SPI trasmission in master...
Posted on August 05, 2004 at 17:19Hi, i have working differences in InDart with a st7lite09. I have build a program that has to send some bytes by SPI (exactly it's not connected in a SPI sistem, but now the chip works single: just for a preliminary...
Posted on July 28, 2004 at 10:51Hi to everybody, i'd like to make a sipmle MIDI piano that should be connected to my computer. Which ST7 have implemented the MIDI serial protocol? I thank you
Posted on July 19, 2004 at 07:08Pardon, i'm a beginner. The CPU Frequency is equal to the RC oscillator? (In the st7lite09 there is an internal RC Oscillator (1 MHz): is the CPU Frequency at 1 MHz?) I need a baud rate of 31250 with a st7lite09. I ca...