Posted on May 17, 2011 at 10:17Looks like a bad Max232 chip. With the logic analyzer I can see data going into the 232 level converter chip, but nothing going out to the mpu. Joy, another month to get a replacement board? I ordered a handful of 232 ...
Posted on May 17, 2011 at 10:17Hello, I've got a EVAL6208PD board with Practispin ST7 based driver board. Problem is I can't get the Practispin software to speak to the ST7 board over RS-232. The board has 5V (5.01V) coming from the 6208PD board and...